Library Components
This section provides information on the library components, which are used for monitoring the power system.
The various library components include:
- Circuit Breaker
 - Motor
 - Switch
 - Automatic Transfer Switch
 - Lockout/Tagout
 - Generator
 - Transformer
 - Utilities
 - Busbar
 
There are two prevailing standards for electrical equipment:
- ANSI
 - IEC
 
NOTE: The color codes shown in the graphic representations of bind properties for various library components depend on the Advanced One Line (AOL) configuration.